PD-I
English
Information about the documentation
Conventions
Warning signs
The following warning signs are used:![]() |
DANGER! Draws attention to imminent danger that will lead to serious personal injury or fatality. |
![]() |
WARNING! Draws attention to a potentially dangerous situation that could lead to serious personal injury or fatality. |
![]() |
CAUTION! Draws attention to a potentially dangerous situation that could lead to slight personal injury or damage to the equipment or other property. |
Symbols
The following symbols are used:![]() |
Read the operating instructions before use. |
![]() |
On/off button |
![]() |
“Measure” button |
![]() |
Menu button |
![]() |
Delete (clear) button |
![]() |
Right arrow button |
![]() |
Left arrow button |
Typographical emphasis
The following typographic features are used to emphasize important passages in this technical documentation:1 |
These numbers refer to the corresponding illustrations. |
About this documentation
- It is essential that the operating instructions are read before initial operation.
- The information provided in the detailed operating instructions installed in the tool as well as the supplements and updates provided at www.hilti.com must also be observed.
- Always keep these operating instructions together with the tool.
- Ensure that the operating instructions are with the tool when it is given to other persons.
Product information
Hilti products are designed for professional use and may be operated, serviced and maintained only by trained, authorized personnel. This personnel must be informed of any particular hazards that may be encountered. The product and its ancillary equipment may present hazards when used incorrectly by untrained personnel or when used not as directed.The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to enquire about the product.
Product information
Laser range meter |
PD-I |
Generation |
01 |
Serial no. |
Laser information on the tool
Laser informationLaser information
![]() |
Laser Class 2 based on the IEC60825-1 / EN60825-1:2007 standard in compliance with CFR 21 § 1040 (Laser Notice 50). |
![]() |
Laser Class 2: Do not stare into the beam. Do not direct the beam toward other persons or toward areas in which other persons, who are not involved in the work with lasers, may be present. |
![]() |
Recycle waste material. |
Safety
Safety instructions
Basic information concerning safety
In addition to the safety rules listed in the individual sections of these operating instructions, the following rules must be strictly observed at all times. The product and its ancillary equipment may present hazards when used incorrectly by untrained personnel or when used not as directed.- Keep all safety instructions and information for future reference.
- Stay alert, watch what you are doing and use common sense when working with the product. Do not use the product while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating the product may result in serious personal injury.
- Do not render safety devices ineffective and do not remove information and warning notices.
- If the product is opened improperly, laser radiation in excess of Class 2 may be emitted. Have the product repaired only by Hilti Service.
- Tampering with or modification of the product is not permitted.
- Check that the product functions correctly each time before use.
- Measurements taken through panes of glass or other objects may be inaccurate.
- The measurement may be incorrect if the conditions under which the measurement is taken change rapidly, e.g. due to people walking through the path of the laser beam.
- Do not point the product toward the sun or other powerful light sources.
- Take the influences of the surrounding area into account. Do not use the tool where there is a risk of fire or explosion.
- Observe the information printed in the operating instructions concerning operation, care and maintenance.
General safety rules
- Check the product for damage before use. Have the damage repaired by Hilti Service.
- Check the accuracy of the product after it has been dropped or subjected to other mechanical stresses.
- Although the product is designed for the tough conditions of jobsite use, as with other measuring instruments it should be treated with care.
- Products which are not in use must be stored in a dry, high place or locked away out of reach of children.
- The product is not intended for use by children.
- Observe the national health and safety requirements.
Proper preparation of the working area
- Avoid unfavorable body positions when working from ladders. Make sure you have a safe stance and that you stay in balance at all times.
- Secure the site at which you are taking measurements and take care to avoid directing the laser beam toward other persons or toward yourself.
- When the product is brought into a warm environment from very cold conditions, or vice-versa, allow it to become acclimatized before use.
- Use the product only within its specified limits.
- Keep the laser exit window clean in order to avoid measurement errors.
- Observe the accident prevention regulations applicable in your country.
Working safely with laser tools
- Laser Class 2/Class II tools may be operated only by appropriately trained persons.
- Laser beams should not be projected at eye height.
- Precautions must be taken to ensure that the laser beam does not unintentionally strike highly reflective surfaces.
- Precautions must be taken to ensure that persons do not stare directly into the beam.
- The laser beam must not be allowed to project beyond the controlled area.
- Switch the laser tool off when it is not in use.
- Store laser tools, when not in use, in places to which unauthorized persons have no access.
Electromagnetic compatibility
Although the device complies with the strict requirements of the applicable directives, Hilti cannot entirely rule out the possibility of interference to the device caused by powerful electromagnetic radiation, possibly leading to incorrect operation. Check the accuracy of the device by taking measurements by other means when working under such conditions or if you are unsure. Likewise, Hilti cannot rule out the possibility of interference with other devices (e.g. aircraft navigation equipment). The tool complies with the requirements of class A; The possibility of interference occurring in a domestic environment cannot be excluded.Only for Korea: This laser range meter is suitable for commercial and industrial use and for the electromagnetic radiation encountered in this field (Class A). Users must pay attention to this point and make sure that this laser range meter is not used in occupied living areas.
Description
Overview of the product

- Rear contact surface
- Reference indicator LED for rear contact
- Left arrow button
- Menu button
- “Measure” button
- Graphic display
- Reference indicator LED for front contact
- On/off button
- Right arrow button
- Hand strap attachment point
- Delete (clear) button
- ¹/₄ inch thread
- Folding spike
- Laser emitting and receiving lens
- ¹/₄ inch thread
Intended use
The product described is a laser range meter. It is designed for taking individual measurements as well as the continuous measurement of distances.
Distances can be measured from all stationary targets without a highly reflective surface, i.e. concrete, stone, wood, plastic, paper, etc. The use of prisms or other highly reflective targets is not permissible and, if attempted, may falsify the results.The product is approved for use with batteries of the type AAA.
Explanation of the display
Main menu![]() |
Measure volumes |
![]() |
Measure rectangular areas |
![]() |
Select layout function |
![]() |
Measure areas and volumes |
![]() |
Select special functions |
![]() |
Select trapezoid function |
![]() |
Select Pythagoras function |
![]() |
Select settings At least one right angle is required for horizontal and diagonal distances. |
![]() |
Select indirect measuring No specific angle is required for measurements on non-moving objects such as walls. |
![]() |
Battery charge state |
![]() |
Measuring spike not folded out |
![]() |
Measuring spike folded out |
![]() |
Measuring |
![]() |
Adding distances |
![]() |
Subtracting distances |
![]() |
Select |
![]() |
Do not select |
![]() |
Select measuring time |
![]() |
Select calculator |
![]() |
Measuring rectangular areas |
![]() |
Measuring triangular areas |
![]() |
Measuring volumes |
![]() |
Measuring cylinder volume |
![]() |
Select automatic brightness sensor |
![]() |
Select min/max delta function |
![]() |
Select layout function |
![]() |
Determine painter’s area |
![]() |
Select timer |
![]() |
Select offset function |
![]() |
Select data storage media |
![]() |
Measure 3 distances |
![]() |
Measure 2 distances, 1 angle |
![]() |
Single Pythagoras |
![]() |
Double Pythagoras |
![]() |
Combined Pythagoras |
![]() |
Unit of measurement. Select unit of measurement:![]() ![]() ![]() |
![]() |
Measuring references. Select measuring reference: ![]() ![]() ![]() |
![]() |
Angle unit. Select angle unit: ![]() ![]() ![]() ![]() |
![]() |
Select expert mode |
![]() |
Edit favorites list |
![]() |
Activate scale |
![]() |
Switching the signal tone on / off |
![]() |
Select laser on constantly |
![]() |
Select display inclination |
![]() |
Calibrate inclination sensor |
![]() |
Display information about the tool |
![]() |
Resetting to the default settings |
![]() |
Indirect horizontal distance measurement |
![]() |
Indirect vertical distance measurement |
![]() |
Measurements on ceilings |
Items supplied
Laser range meter, two batteries, operating instructions, manufacturer’s certificate.Technical data
Battery life |
Room temperature: Up to 5000 measurements |
Operating temperature |
−10 ℃ … 50 ℃ (14 ℉ … 122 ℉) |
Distance measurement accuracy (2σ, standard deviation) |
±1.0 mm |
Inclination measurement accuracy (2σ, standard deviation) |
±0.2° |
Weight (including batteries) |
165 g (5.8 oz) |
Storage temperature |
−30 ℃ … 70 ℃ (−22 ℉ … 158 ℉) |
Laser class in accordance with EN 60825-1:2007 |
Laser class 2 |
Protection class in accordance with IEC 60529 |
IP 65 |
Power source |
1.5 V |
Operation
Basic functions
Navigate to the desired function with the aid of the left or right arrow buttons.- Always press the “Measure” button to select a function.
Inserting the batteries

- Open the battery compartment and insert the batteries.
Switching the laser range meter on and off
- If the tool is switched off, press the on/off button or the “Measure” button to switch it on.
- If the tool is switched on, press the on/off button to switch it off.
Measuring using the spike

- Fold out the spike through 90°. The spike can then be used as the contact point.
- Fold out the spike through 180°. The measuring reference point is then set automatically.
Measuring using a target plate

- Use the target plate to measure distance under the following unfavorable conditions:
- The wall is not sufficiently reflective due to the type of surface.
- The target point is not on a surface.
- The distance to be measured is very long.
- The light conditions are unfavorable (bright sunshine).
- The wall is not sufficiently reflective due to the type of surface.
- A distance of 1.2 mm should be added to the measured distance when using a target plate.
Single measurements
- Press the “Measure” button briefly to activate the laser beam.
- Keep the laser beam on the target point.
- Press the “Measure” button briefly to take the measurement.
- The measured distance is shown in the lower line of the display.
- The distance measured in the previous measurement is shown in the upper line of the display.
- The measured distance is shown in the lower line of the display.
- To take another measurement, keep the laser beam on the target point and press the “Measure” button again.
Continuous measurement
- Press the “Measure” button for 2 seconds.
- If the signal tone is active, a signal tone will be emitted.
- If the signal tone is active, a signal tone will be emitted.
- Move the laser range meter toward or away from the target until the desired distance is reached.
- Press the “Measure” button briefly.
- The measured distance is shown in the lower line of the display.
- The distance measured in the previous measurement is shown in the upper line of the display.
- The measured distance is shown in the lower line of the display.
Measuring volumes
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Measuring rectangular areas
- Aim the tool at the target point for the room width and press the “Measure” button.
- Aim the tool at the target point for the room length and press the “Measure” button.
Layout function
- Enter the distance manually. Do this by using the left or right arrow buttons to select the keyboard symbol and confirm by pressing the “Measure” button.
- Select the applicable numbers and confirm by pressing the “Measure” button.
- To confirm the value, select the check mark symbol (tick) at the bottom right corner.
- Select the flag symbol.
- The distance you have entered will then be shown between the two flags.
- The distance you have entered will then be shown between the two flags.
- Press the “Measure” button to begin measuring.
- The arrows on the screen indicate in which direction you must move the tool. When the target distance is reached, black arrows appear above and below the distance shown in the display.
- The arrows on the screen indicate in which direction you must move the tool. When the target distance is reached, black arrows appear above and below the distance shown in the display.
- To repeat this distance measurement several times, move the tool further. The number of times you have measured out this distance is shown on the right of the screen.
- Press the “Measure” button to stop measuring.
Special functions
Automatic brightness sensor
- Select the symbol for the automatic brightness sensor from the special functions menu.
Min/max delta function
- Select the symbol for the min/max delta function from the special functions menu.
- Aim the tool at the target point and press the “Measure” button.
- Press the “Measure” button to stop measuring.
- The last distances measured are shown in the results line.
- The last distances measured are shown in the results line.
Painter’s area
- Aim the tool at the target point for the first room length and press the “Measure” button.
- The result is saved as an intermediate result.
- The result is saved as an intermediate result.
- Aim the tool at the target for the next room length and press the “Measure” button to take the measurement.
- The second result is shown in the intermediate results table. The intermediate result shown in bold is the sum of the measured room lengths.
- The second result is shown in the intermediate results table. The intermediate result shown in bold is the sum of the measured room lengths.
- Repeat this procedure until all room lengths have been measured.
- Press the right arrow button to switch to room height and confirm by pressing the “Measure” button.
- Position and aim the tool for room height measurement and then take the measurement.
- The room height is measured and displayed in the intermediate result line. The painter’s area is calculated immediately and shown in the result line.
- The room height is measured and displayed in the intermediate result line. The painter’s area is calculated immediately and shown in the result line.
Timer
- Select the timer symbol from the special functions menu.
- Set the timer to 2, 5 or 10 seconds and confirm by pressing the “Measure” button.
- Select the “Measure” symbol to trigger the delayed measurement.
Data memory
- Select the data storage symbol from the special functions menu.
- To delete data storage memory, press and hold the C-button for 2 seconds while the data storage screen is displayed.
Trapezoid
Trapezoid function (3 distances)
- Select the symbol for the trapezoid function for 3 distances from the trapezoid functions menu.
- Aim the tool at the target point and press the “Measure” button.
- After measuring the first distance, the graphical display automatically prompts you to take the next measurement.
- After measuring the first distance, the graphical display automatically prompts you to take the next measurement.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the third target point and press the “Measure” button.
Trapezoid with Inclination (2 distances, 1 angle)
- Select the symbol for the trapezoid function with inclination from the trapezoid functions menu.
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Pythagoras
Single Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Double Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the third target point and press the “Measure” button.
Combined Pythagoras
- Aim the tool at the target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
- Aim the tool at the next target point and press the “Measure” button.
Settings
Editing the favorites list
- Navigate to the function that you wish to edit and confirm by pressing the “Measure” button.
- Navigate to the desired function and confirm by pressing the “Measure” button.
Activating the scale
- Set the applicable number and confirm the value by pressing the “Measure” button.
- Select the check mark symbol (tick) to confirm the value.
Calibrate inclination sensor
- Place the tool on a horizontal surface and press the “Measure” button.
- Rotate the tool through 180° and press the “Measure” button.
- The inclination sensor is now calibrated.
- The inclination sensor is now calibrated.
Indirect measurements
Indirect horizontal distance measurement
- Aim the tool at the target point and press the “Measure” button.
- The distance and angle of inclination are measured and shown in the intermediate result line.
- The target distance is calculated immediately and shown in the result line.
- The distance and angle of inclination are measured and shown in the intermediate result line.
Indirect vertical distance (2 angles, 2 distances)
- Aim the tool at the target point and press the “Measure” button.
- The first distance and angle are measured and shown in the intermediate result line.
- The graphical display automatically prompts you to measure the second distance.
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
- The target distance is calculated immediately and shown in the result line.
- The target distance is calculated immediately and shown in the result line.
Measuring on ceilings
- Aim the tool at the target point and press the “Measure” button.
- The first distance and angle are measured and shown in the intermediate result line.
- The graphical display automatically prompts you to measure the second distance.
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
- The target distance is calculated immediately and shown in the result line.
- The target distance is calculated immediately and shown in the result line.
Indirect vertical distance II (2 angles, 1 distance)
- Aim the tool at the target point and press the “Measure” button.
- The first distance and angle are measured and shown in the intermediate result line.
- The graphical display automatically prompts you to measure the second distance.
- The first distance and angle are measured and shown in the intermediate result line.
- Aim the tool at the next target point and press the “Measure” button.
- The target distance is calculated immediately and shown in the result line.
- The target distance is calculated immediately and shown in the result line.
Care, transport and storage
Cleaning
- Do not touch the lens with the fingers.
- Clean the lens by blowing the dust off or by wiping with a clean, dry cloth.
- Do not use liquids other than pure alcohol or water.
Transport
- Use the Hilti packaging or packaging of equivalent quality for transporting or shipping your equipment.
Storage and drying
- Do not put the product into storage when wet. Allow it to dry before putting it away.
- Observe the temperature limits given in the Technical Data section which are applicable to storage or transport of the equipment.
- Check the accuracy of the equipment before it is used after a long period of storage or transportation.
Disposal

In accordance with the European Directive on waste electrical and electronic equipment and its implementation in conformance with national law, electric tools or appliances that have reached the end of their life must be collected separately and returned to an environmentally compatible recycling facility.
FCC statement / IC statement
CAUTION This product has been tested and found to comply with the limits for a class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. These products generate, use and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause interference to radio communications.There is no guarantee that interference will not occur in a particular installation. If this product does cause harmful interference to radio or television reception, which can be determined by turning the product off and on, the user is encouraged to try to correct the interference by taking the following measures:
- Re-orient or move the receiving antenna.
- Increase the distance between the product and receiver.
- Connect the product to a power outlet on a circuit different from that to which the receiver is connected.
- Consult your dealer or an experienced TV/radio technician for assistance.
This product complies with the requirements in Paragraph 15 of the FCC Rules and RSS 210 of IC.
Operation of the product is subject to the following conditions:
- This product should cause no harmful interference.
- This product must accept any interference received, including interference that may cause undesired operation.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.