NPU 100 IP-A22
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols used
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the documentation
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
Symbols on the power tool
Symbols
The following symbols are used:![]() |
Risk of cutting injury! |
![]() |
Wear protective glasses! |
![]() |
Wireless data transfer |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationHole punch NPU 100 IP-A22 Generation 01 Serial no.
Declaration of conformity
We declare, on our sole responsibility, that the product described here complies with the applicable directives and standards. A copy of the declaration of conformity can be found at the end of this documentation.The technical documentation is filed here:
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
- Do not operate power tools in explosive atmospheres, such as in the presence of flammable liquids, gases or dust. Power tools create sparks which may ignite the dust or fumes.
- Keep children and bystanders away while operating a power tool. Distractions can cause you to lose control.
- Power tool plugs must match the outlet. Never modify the plug in any way. Do not use any adapter plugs with earthed (grounded) power tools. Unmodified plugs and matching outlets will reduce risk of electric shock.
- Avoid body contact with earthed or grounded surfaces, such as pipes, radiators, ranges and refrigerators. There is an increased risk of electric shock if your body is earthed or grounded.
- Do not expose power tools to rain or wet conditions. Water entering a power tool will increase the risk of electric shock.
- Do not abuse the cord. Never use the cord for carrying, pulling or unplugging the power tool. Keep cord away from heat, oil, sharp edges or moving parts. Damaged or entangled cords increase the risk of electric shock.
- When operating a power tool outdoors, use an extension cord suitable for outdoor use. Use of a cord suitable for outdoor use reduces the risk of electric shock.
- If operating a power tool in a damp location is unavoidable, use a residual current device (RCD) protected supply. Use of an RCD reduces the risk of electric shock.
- Stay alert, watch what you are doing and use common sense when operating a power tool. Do not use a power tool while you are tired or under the influence of drugs, alcohol or medication. A moment of inattention while operating power tools may result in serious personal injury.
- Use personal protective equipment. Always wear eye protection. Protective equipment such as a dust mask, non-skid safety shoes, hard hat or hearing protection used for appropriate conditions will reduce personal injuries.
- Prevent unintentional starting. Ensure the switch is in the off-position before connecting to power source and/or battery pack, picking up or carrying the tool. Carrying power tools with your finger on the switch or energising power tools that have the switch on invites accidents.
- Remove any adjusting key or wrench before turning the power tool on. A wrench or a key left attached to a rotating part of the power tool may result in personal injury.
- Do not overreach. Keep proper footing and balance at all times. This enables better control of the power tool in unexpected situations.
- Dress properly. Do not wear loose clothing or jewellery. Keep your hair, clothing and gloves away from moving parts. Loose clothes, jewellery or long hair can be caught in moving parts.
- If devices are provided for the connection of dust extraction and collection facilities, ensure these are connected and properly used. Use of dust collection can reduce dust-related hazards.
- Do not let familiarity gained from frequent use of tools allow you to become complacent and ignore tool safety principles. A careless action can cause severe injury within a fraction of a second.
- Do not force the power tool. Use the correct power tool for your application. The correct power tool will do the job better and safer at the rate for which it was designed.
- Do not use the power tool if the switch does not turn it on and off. Any power tool that cannot be controlled with the switch is dangerous and must be repaired.
- Disconnect the plug from the power source and/or remove the battery pack, if detachable, from the power tool before making any adjustments, changing accessories, or storing power tools. Such preventive safety measures reduce the risk of starting the power tool accidentally.
- Store idle power tools out of the reach of children and do not allow persons unfamiliar with the power tool or these instructions to operate the power tool. Power tools are dangerous in the hands of untrained users.
- Maintain power tools and accessories. Check for misalignment or binding of moving parts, breakage of parts and any other condition that may affect the power tool’s operation. If damaged, have the power tool repaired before use. Many accidents are caused by poorly maintained power tools.
- Keep cutting tools sharp and clean. Properly maintained cutting tools with sharp cutting edges are less likely to bind and are easier to control.
- Use the power tool, accessories and tool bits etc. in accordance with these instructions, taking into account the working conditions and the work to be performed. Use of the power tool for operations different from those intended could result in a hazardous situation.
- Keep handles and grasping surfaces dry, clean and free from oil and grease. Slippery handles and grasping surfaces do not allow for safe handling and control of the tool in unexpected situations.
- Recharge only with the charger specified by the manufacturer. A charger that is suitable for one type of battery pack may create a risk of fire when used with another battery pack.
- Use power tools only with specifically designated battery packs. Use of any other battery packs may create a risk of injury and fire.
- When battery pack is not in use, keep it away from other metal objects, like paper clips, coins, keys, nails, screws or other small metal objects, that can make a connection from one terminal to another. Shorting the battery terminals together may cause burns or a fire.
- Under abusive conditions, liquid may be ejected from the battery; avoid contact. If contact accidentally occurs, flush with water. If liquid contacts eyes, additionally seek medical help. Liquid ejected from the battery may cause irritation or burns.
- Do not use a battery pack or tool that is damaged or modified. Damaged or modified batteries may exhibit unpredictable behaviour resulting in fire, explosion or risk of injury.
- Do not expose a battery pack or tool to fire or excessive temperature. Exposure to fire or temperature above 130° C (265 °F) may cause explosion.
- Follow all charging instructions and do not charge the battery pack or tool outside the temperature range specified in the instructions. Charging improperly or at temperatures outside the specified range may damage the battery and increase the risk of fire.
- Have your power tool serviced by a qualified repair person using only identical replacement parts. This will ensure that the safety of the power tool is maintained.
- Never service damaged battery packs. Service of battery packs should only be performed by the manufacturer or authorized service providers.
Additional safety instructions applicable to hole punches
Personal safety- Use the product only if it is in perfect working order.
- Never tamper with or modify the tool in any way.
- Before use of the power tool, all live cables or other items carrying electric voltage within the area in which the user is working are to be switched off. If this is not possible, the corresponding safety precautions for working in the proximity of live cables or equipment must be implemented and observed.
- Do not punch live parts.
- After punching approx. 30 to 40 consecutive holes, switch the power tool off and allow it to cool down for about 15 minutes. Overheating can lead to damage to the power tool.
Battery use and care
- Observe the special regulations and instructions applicable to the transport, storage and use of Li-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti Service .
- If the battery is too hot to touch it may be defective. In this case, place the product in a non-flammable location, well away from flammable materials, where it can be kept under observation and allowed to cool down. In this case, always contact your Hilti Service .
Description
Product overview

- Punching head
- Manual piston return switch
- Casing
- Servicing and fault indicator (red LED)
- Battery release button
- Battery
- Slot on both sides to fasten the Hilti retaining leash
- White LED to illuminate the working area
- Control switch
Intended use
The product described is a cordless electro-hydraulic punching tool. It is designed for punching round, square and rectangular holes in steel, aluminum, plastic or fiberglass parts.
Use only the punching dies available through the manufacturer.Before starting work, check that the sheets to be punched and everything in the work zone (e.g. distribution box/switch cabinet) are not electrically live.
Use only Hilti lithium‑ion batteries of the B 22 series with this product.
Use only Hilti battery chargers of the C4/36 series for charging these batteries.
Possible misuse
- Do not use this hand-held power tool clamped in a fixed position or as a stationary device.
- Do not punch electrically live parts.
Lithium‑ion battery status display
The state of charge of the Li-ion battery and malfunctions of the power tool are indicated by the display on the Li‑ion battery. The state of charge of the Li‑ion battery is displayed after pressing one of the two battery release buttons.Status |
Meaning |
---|---|
4 LEDs light. |
State of charge: 75 % to 100 % |
3 LEDs light. |
State of charge: 50 % to 75 % |
2 LEDs light. |
State of charge: 25 % to 50 % |
1 LED lights. |
State of charge: 10 % to 25 % |
1 LED blinks. |
State of charge: < 10 % |
Items supplied
Hole punch, operating instructions.Other system products approved for use with this product can be found at your local Hilti Store or online at: www.hilti.group | USA: www.hilti.com .
Technical data
NPU 100 IP-A22 |
|
---|---|
Rated voltage |
21.6 V |
Weight in accordance with EPTA procedure 01 |
3.02 kg |
Max. punching capacity in 10 ga steel |
4" |
Max. punching capacity in 10 ga steel |
4" |
Storage temperature |
−20 ℃ … 70 ℃ |
Ambient temperature for operation |
−17 ℃ … 60 ℃ |
Noise and vibration values in accordance with EN 60745
The sound pressure and vibration values given in these instructions were measured in accordance with a standardized test and can be used to compare one power tool with another. They can also be used for a preliminary assessment of exposure. The data given represents the main applications of the power tool. However, if the power tool is used for different applications, with different accessory tools, or is poorly maintained, the data can vary. This can significantly increase exposure over the total working period. An accurate estimation of exposure should also take into account the times when the power tool is switched off, or when it is running but not actually being used for a job. This can significantly reduce exposure over the total working period. Identify additional safety measures to protect the operator from the effects of noise and/or vibration, for example: maintaining the power tool and accessory tools, keeping the hands warm, organization of work patterns.Noise values
Sound (power) level (L WA) |
80 dB(A) |
Uncertainty for the sound power level (K WA) |
2.5 dB(A) |
Emission sound pressure level (L pA) |
70 dB(A) |
Uncertainty for the sound pressure level (K pA) |
2.5 dB(A) |
Total vibration (during operation) (a) |
2.5 m/s² |
Uncertainty (K) |
1.5 m/s² |
Battery
Battery operating voltage |
21.6 V |
Ambient temperature for operation |
−17 ℃ … 60 ℃ |
Storage temperature |
−20 ℃ … 40 ℃ |
Battery charging starting temperature |
−10 ℃ … 45 ℃ |
Operation
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the battery holder until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the release buttons on the battery.
- Pull the battery out of its holder in the device.
Assemble Hilti retaining leash (optional)

- Remove the battery.
- Insert the two tabs on the retaining leash into the slots on each side of the base.
- Secure the retaining leash with the screws supplied.
- Refit the battery.
Dismantle the Hilti retaining leash (optional)

- Remove the battery.
- Remove the two retaining strap securing screws.
- Pull the two retaining strap tabs out of the slots in the base and remove the retaining strap.
- Refit the battery.
Observing the safety instructions
- It is essential that the safety instructions are observed.
Punching holes up to 4"

- Determine the exact position of the hole. To predrill the hole, use a drill bit of a diameter slightly larger than that of the draw stud.
- Select the required punch.
- Select the corresponding die.
- Select the required draw stud.
- Check that the piston in the tool is fully retracted. Assemble the complete punching set, making sure that the cutting side of the punch is facing the sheet metal. Screw the punch in so that it makes light contact with the sheet metal.
- Insert the battery.
- Press and hold the control switch until the punching operation is automatically completed.
Care and maintenance
Care and maintenance of the tool- Carefully remove stubborn dirt.
- Clean the air vents carefully with a dry brush.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Keep the battery free from oil and grease.
- Use only a slightly damp cloth to clean the casing. Do not use cleaning agents containing silicone as these may attack the plastic parts.
- Avoid ingress of moisture.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not operate the product if signs of damage are found or if parts malfunction. Have it repaired immediately by Hilti Service.
- After cleaning and maintenance, fit all guards or protective devices and check that they function correctly.
Transport and storage of cordless tools
Transport- Remove the battery.
- Never transport batteries in bulk form (loose, unprotected).
- Check the tool and batteries for damage before use after long periods of transport.
- Store the tool and batteries in a place that is as cool and dry as possible.
- Never store batteries in direct sunlight, on heating units or behind a window pane.
- Store the tool and batteries in a place where they cannot be accessed by children or unauthorized persons.
- Check the tool and batteries for damage before use after long periods of storage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, please contact Hilti Service.The punching tool is not in working order.
Malfunction |
Possible cause |
Action to be taken |
---|---|---|
The LEDs on the battery indicate nothing. |
The battery is not correctly inserted. |
|
The battery is discharged. |
|
|
The battery is too hot or too cold. |
|
|
1 LED on the battery blinks. |
The battery is discharged. |
|
The battery is too hot or too cold. |
|
|
4 LEDs on the battery blink. |
Product momentarily overloaded. |
|
Red LED => lights continuously and a warning tone is emitted. |
Technical problem. |
|
Red LED => blinks at short intervals and a warning tone is emitted. |
The state of charge of the battery is too low to allow a complete operating cycle. |
|
Red LED => lights briefly and no warning tone is emitted. |
Product overheated. |
|
The punching tool is in working order.
Trouble or fault |
Possible cause |
Action to be taken |
---|---|---|
The battery runs down more quickly than usual. |
Very low ambient temperature. |
|
The battery does not engage with an audible double click. |
The retaining lugs on the battery are dirty. |
|
Red LED => lights continuously and a warning tone is emitted. |
Technical problem. |
|
Disposal

Battery disposalImproper disposal of batteries can result in health hazards from leaking gases or fluids.
- DO NOT send batteries through the mail!
- Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.
- Dispose of your battery out of the reach of children.
- Dispose of the battery at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions.
RoHS (Restriction of Hazardous Substances)
Click on the link to go to the table of hazardous substances: qr.hilti.com/r7794537.There is a link to the RoHS table, in the form of a QR code, at the end of this document.
Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.