R 6-22
Original operating instructions
Information about the documentation
About this documentation
- Read this documentation before initial operation or use. This is a prerequisite for safe, trouble-free handling and use of the product.
- Observe the safety instructions and warnings in this documentation and on the product.
- Always keep the operating instructions with the product and make sure that the operating instructions are with the product when it is given to other persons.
Explanation of symbols
Warnings
Warnings alert persons to hazards that occur when handling or using the product. The following signal words are used:Symbols in the operating instructions
The following symbols are used in these operating instructions:![]() |
Comply with the operating instructions |
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
Hilti Li‑ion battery |
![]() |
Hilti charger |
Symbols in illustrations
The following symbols are used in illustrations:![]() |
These numbers refer to the illustrations at the beginning of these operating instructions. |
![]() |
The numbering reflects the sequence of operations shown in the illustrations and may deviate from the steps described in the text. |
![]() |
Item reference numbers are used in the overview illustration and refer to the numbers used in the key in the product overview section. |
![]() |
These characters are intended to specifically draw your attention to certain points when handling the product. |
Product-dependent symbols
Symbols on the product
The following symbols can be used on the product:![]() |
Protection class II (double-insulated) |
![]() |
Only use in enclosed spaces |
![]() |
The power tool supports near-field communication (NFC) technology, which is compatible with iOS and Android platforms. |
![]() |
Hilti Li-ion battery type series used. Observe the information given in the section headed Intended use . |
![]() |
Li-ion battery |
![]() |
If applied on the product, the product has been certified by this certification body for the US and Canadian markets according to the applicable standards. |
Product information

The type designation and serial number are printed on the rating plate.
- Write down the serial number in the table below. You will be required to state the product details when contacting Hilti Service or your local Hilti organization to inquire about the product.
Product informationRadio R 6-22 Generation 01 Serial no.
Declaration of conformity

The technical documentation is filed here:
Hilti Entwicklungsgesellschaft mbH | Tool Certification | Hiltistrasse 6 | D-86916 Kaufering, Germany
Safety
General safety instructions
ATTENTION! Read all instructions. Failure to follow all instructions listed below may result in electric shock, fire and/or serious injury.Keep these instructions in a handy yet secure place.
Workplace
- Ensure that the workplace is well lit.
- Do not tamper with or attempt to make alterations to the appliance.
- The appliance is not intended for wall mounting.
- Keep your work area clean and well lit. Cluttered or poorly lit work areas invite accidents.
- This product is not intended for use by persons (including children) with physical, sensory or mental disabilities or persons lacking the appropriate experience and/or knowledge. These persons must receive instruction in safe handling of the appliance and must be supervised throughout their use of the appliance by a responsible person.
- Explain to children that they are not allowed to play with the appliance.
- Children over 8 years of age must receive instruction in safe handling of the appliance and must be supervised throughout their use of the appliance by a responsible person.
- Do not wear jewelry such as rings or chains. Jewelry could cause a short circuit resulting in personal injury in the form of burns.
- Avoid touching the contacts.
- Observe the special guidelines applicable to the transport, storage and use of Li-ion batteries.
- Do not expose batteries to high temperatures, direct sunlight or fire.
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C.
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. In this case, always contact your Hilti Service .
- If the battery is too hot to touch it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Contact Hilti Service .
- Have the appliance serviced by a qualified repair person using only genuine Hilti spare parts. The safety of the appliance can thus be maintained.
Battery use and care
- Comply with the following safety instructions for the safe handling and use of Li-ion batteries. Failure to comply can lead to skin irritation, severe corrosive injury, chemical burns, fire and/or explosion.
- Use only batteries that are in perfect working order.
- Treat batteries with care in order to avoid damage and prevent leakage of fluids that are extremely harmful to health!
- Do not under any circumstances modify or tamper with batteries!
- Do not disassemble, crush or incinerate batteries and do not subject them to temperatures over 80 °C (176 °F).
- Never use or charge a battery that has suffered an impact or been damaged in any other way. Check your batteries regularly for signs of damage.
- Never use recycled or repaired batteries.
- Never use the battery or a battery-operated power tool as a striking tool.
- Never expose batteries to the direct rays of the sun, elevated temperature, sparking, or open flame. This can lead to explosions.
- Do not touch the battery poles with your fingers, tools, jewelry, or other electrically conductive objects. This can damage the battery and also cause material damage and personal injury.
- Keep batteries away from rain, moisture and liquids. Penetrating moisture can cause short circuits, electric shock, burns, fire and explosions.
- Use only chargers and power tools approved for the specific battery type. Read and follow the relevant operating instructions.
- Do not use or store the battery in explosive environments.
- If the battery is too hot to touch, it may be defective. Put the battery in a place where it is clearly visible and where there is no risk of fire, at an adequate distance from flammable materials. Allow the battery to cool down. If it is still too hot to touch after an hour, the battery is faulty. Consult Hilti Service or read the document entitled "Instructions on safety and use for Hilti Li-ion batteries".
Description
Overview

- Display
- Power button
- Carrying handle
- Antenna
- Knob
- Casing
- Rubber armoring
- Mode button
- Preset button
- Bluetooth button
- Equalizer button
- Time settings
- USB port
- AUX port
- Battery
- NFC interface
- Battery compartment
Intended use
The product described is a cordless jobsite radio. It is designed for playing music as a radio receiver or from various other devices that can be either paired with the product via Bluetooth or connected to it by an AUX cable.
The product is designed for a jobsite environment. Do not expose the product to moisture such as running water, for example.
Use the product only indoors.

For this product, use only Hilti lithium‑ion batteries of the B 22 series. For this product, Hilti recommends the use of the batteries stated in this table.
For these batteries, use only Hilti chargers of the type series listed here.
Items supplied
Jobsite radio, AAA batteries (2 of), operating instructionsBluetooth
This product is equipped with Bluetooth (optional).Bluetooth is a wireless data transfer system by which the two Bluetooth-enabled products can communicate with each other over a short distance.
Status indicators of the Li‑ion battery
Hilti Nuron Li-ion batteries can indicate state of charge, fault messages and the battery's state of health.Indicators for state of charge and fault messages
Short-press the release button of the battery to get whichever of the following status indications is applicable at the time.State of charge and, if applicable, faults are indicated constantly as long as the connected product is switched on.
Status |
Meaning |
---|---|
Four (4) LEDs show constantly green |
State of charge: 100 % to 71 % |
Three (3) LEDs show constantly green |
State of charge: 70 % to 51 % |
Two (2) LEDs show constantly green |
State of charge: 50 % to 26 % |
One (1) LED shows constantly green |
State of charge: 25 % to 10 % |
One (1) LED slow-flashes green |
State of charge: < 10 % |
One (1) LED quick-flashes green |
The Li-ion battery is completely discharged. Recharge the battery. If the LED again starts quick-flashing after the battery has been charged, consult Hilti Service. |
One (1) LED quick-flashes yellow |
The Li-ion battery or the product in which it is inserted is overloaded, too hot or too cold, or experiencing some other fault. Bring the product and the battery to the recommended working temperature and do not overload the product when it is in use. If the message persists, consult Hilti Service. |
One (1) LED shows yellow |
The Li-ion battery and the product in which it is inserted are not compatible. Consult Hilti Service. |
One (1) LED quick-flashes red |
The Li-ion battery is locked and cannot be used. Consult Hilti Service. |
Indicators showing the battery's state of health
To check the battery's state of health, press the release button and hold it down for longer than three seconds. The system does not detect a potential malfunction of the battery due to misuse, for example battery dropped or pierced, external heat damage, etc.Status |
Meaning |
---|---|
All LEDs show in sequence, followed by one (1) LED showing constantly green. |
The battery can remain in use. |
All LEDs show in sequence, followed by one (1) LED quick-flashing yellow. |
The check to ascertain the battery's state of health did not complete. Repeat the procedure, or consult Hilti Service. |
All LEDs show in sequence, followed by one (1) LED showing constantly red. |
If a connected product can still be used, the remaining battery capacity is below 50 %. If a connected product can no longer be used, the battery has reached the end of its useful life and has to be replaced. Consult Hilti Service. |
Information shown in the display
Information shown in the displayInformation shown in the display
![]() |
The AM frequency band has been selected as the audio source. |
![]() |
The FM frequency band has been selected as the audio source. |
![]() |
DAB has been selected as the audio source. (Not available in all markets.) |
![]() |
AUX has been selected as the audio source. |
![]() |
Bluetooth has been selected as the audio source. |
![]() |
Mobile device for music playback connected via Bluetooth. The symbol flashes as long the product is searching for a possible connection or is in the process of establishing a connection. |
![]() |
Indicates the bass settings. |
![]() |
Indicates the treble settings. |
![]() |
Indicates stereo playback. Stereo playback is activated automatically when signal reception is good enough. |
![]() |
Indicates the memory slot of the station. |
![]() |
Indicates the time. Symbols flash in setup mode. |
![]() |
DAB reception signal is too weak. |
Cradle for mobile devices

Technical data
Product properties
Power input |
160 W |
Battery operating voltage |
22 V |
Battery pack |
Li-Ion |
Weight (Without battery) |
5.1 kg |
AM frequency range |
526.5 kHz …1,606.5 kHz |
FM frequency range |
87.5 MHz …108 MHz |
DAB / DAB+ |
174 MHz …240 MHz |
USB output voltage |
5.0 V / 2.1 A |
Ambient temperature |
−17 ℃ …40 ℃ |
Bluetooth
Bluetooth radiant power |
7.30 dBm |
Bluetooth frequency |
2,402 MHz …2,480 MHz |
Battery
Battery operating voltage |
21.6 V |
Weight, battery |
See the section headed "Intended use" |
Ambient temperature for operation |
−17 ℃ …60 ℃ |
Storage temperature |
−20 ℃ …40 ℃ |
Battery charging starting temperature |
−10 ℃ …45 ℃ |
Preparations at the workplace
Observe the safety instructions and warnings in this documentation and on the product.Charging the battery
- Before charging the battery, read the operating instructions for the charger.
- Make sure that the contacts on the battery and the contacts on the charger are clean and dry.
- Use an approved charger to charge the battery.
Inserting the battery
- Charge the battery fully before using it for the first time.
- Push the battery into the product until it engages with an audible click.
- Check that the battery is seated securely.
Removing the battery
- Press the battery release button.
- Remove the battery from the product.
Inserting the back-up batteries

- Remove the cover from the battery compartment.
- Insert the 2 AAA batteries supplied with the appliance into the battery compartment.
- Install the cover on the battery compartment.
Switching the appliance on / off

- Press the Power button.
Operation
Observe the safety instructions and warnings in this documentation and on the product.Establishing a Bluetooth connection

- Press the Bluetooth button.
- To initially pair the radio manually, press the Bluetooth button and hold it down for 2 seconds.
- The Bluetooth symbol flashes.
- Select the Hilti radio on the mobile device.
- The devices have been successfully paired when the Bluetooth and pairing symbols both show continuously in the display.
- The Bluetooth symbol flashes.
- If the radio has already been paired to the mobile device, press the Bluetooth button.
- Pairing starts automatically and the pairing symbol on the screen starts to flash.
- The radio searches for a signal for a maximum of 3 minutes.
- The pairing symbol appears on the display to indicate that the devices are paired.
- The Bluetooth symbol appears in the display to indicate that the radio has found a paired mobile device.
- Pairing starts automatically and the pairing symbol on the screen starts to flash.
- If you have a second radio, you can synchronize the two radios and listen to music in stereo.
- Radio (A) is connected to your mobile device. This radio is the master.
- Switch radio (B) on.
- On radio (B) , press the Bluetooth button.
- On master radio (A) , press the Preset button (an acoustic signal sounds to confirm that the connection has been established).
- Shortly after, music will start playing in stereo on the two radios.
- Radio (A) is connected to your mobile device. This radio is the master.
Making an NFC connection

- Activate the NFC function on your mobile device (if it supports NFC).
- Hold you mobile device close to the NFC interface of the radio. This is on the right-hand side and is indicated by the NFC symbol.
Setting the audio source

- Press the mode button.
- Select the desired audio source.
Searching for and saving stations

- Use the knob to select a frequency.
- Press the 'Preset' button.
- Press the knob to save this frequency.
Positioning the antenna

- Swivel the antenna to the position at which reception is clearest.
Adjusting the volume

- Turn the power button clockwise to increase the volume.
- Turn the power button counterclockwise to reduce the volume.
Equalizer settings

- Press the equalizer button (EQ) .
- Use the knob to select either bass or treble for adjustment.
- Use the knob to change your settings.
Audio playback from a mobile device via Bluetooth
- Establish a Bluetooth connection between the mobile device and the radio.
- Select the play mode (Bluetooth).
- Press the Start/Pause button on your mobile device or press the knob to start or pause audio playback.
- Use the arrow buttons on the mobile device or turn the knob to change tracks and to start.
Audio playback from an external device via AUX

- Select the play mode (AUX or Bluetooth).
- Press the start/pause button on your mobile device to start or pause audio playback.
- Use the arrow buttons on the external device to change tracks and to start.
Setting the clock

- Press the clock button.
- Use the knob to set the time.
- Save the time by pressing the knob briefly.
- Use the knob to select whether you wish to synchronize the time and press the knob briefly to confirm your choice.
USB charging function

- Use a USB cable to connect your mobile device to the USB port of the radio.
Care and maintenance
Care of the product- Carefully remove stubborn dirt.
- Carefully clean the air vents, if present, with a dry, soft brush.
- Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Use a dry, clean cloth to clean the contacts of the product.
- Never use a battery with clogged air vents. Clean the air vents carefully using a dry, soft brush.
- Avoid unnecessary exposure of the battery to dust and dirt. Never expose the battery to high levels of moisture (e.g. by being dipped in water or left in the rain).
If a battery has been soaked by moisture, treat it as a damaged battery. Isolate it in a non-flammable container and consult Hilti Service. - Keep the battery free of extraneous oil and grease. Do not permit dust or dirt to accumulate unnecessarily on the battery. Clean the battery with a dry, soft brush or a clean, dry cloth. Do not use cleaning agents containing silicone as these can attack the plastic parts.
Do not touch the contacts of the battery and do not remove the factory-applied grease from the contacts. - Use only a slightly damp cloth to clean the housing. Do not use cleaning agents containing silicone as these can attack the plastic parts.
- Check all visible parts and controls for signs of damage at regular intervals and make sure that they all function correctly.
- Do not use the product if signs of damage are found or if parts malfunction. Immediately have the product repaired by Hilti Service.
- After cleaning and maintenance, install all guards and protective devices and check that they are in full working order.
Transport and storage of cordless tools and batteries
Transport- Remove the battery/batteries.
- Never transport batteries loose and unprotected. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit. Comply with the locally applicable regulations for transporting batteries.
- Do not send batteries through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Prior to each use and before and after prolonged transport, check the product and the batteries for damage.
- Store the product and the batteries in a cool and dry place. Comply with the temperature limits stated in the technical data.
- Do not store batteries on the charger. Always remove the battery from the charger when the charging operation has completed.
- Never leave batteries in direct sunlight, on sources of heat, or behind glass.
- Store the product and batteries where they cannot be accessed by children or unauthorized persons.
- Prior to each use and before and after prolonged storage, check the product and the batteries for damage.
Troubleshooting
If the trouble you are experiencing is not listed in this table or you are unable to remedy the problem by yourself, contact Hilti Service.Malfunction |
Possible cause |
Action to be taken |
---|---|---|
Radio does not switch on. |
Battery discharged |
|
Battery defective |
|
|
Radio defective |
|
|
Border of the battery symbol flashes, no segment of the state of charge indicator filled (the indicator assumes this state for a short time before the appliance switches itself off). |
Battery too hot |
|
Battery too cold |
|
|
Battery defective |
|
|
Settings such as clock time are no longer saved in memory. |
Batteries discharged |
|
Disposal

Manufacturer’s warranty
- Please contact your local Hilti representative if you have questions about the warranty conditions.
Further information
China RoHS (Restriction of Hazardous Substances)
Taiwan RoHS (Restriction of Hazardous Substances)

Hilti Li-ion batteries
Instructions for Use and OperationThis documentation uses the term battery to describe rechargeable Hilti Li-ion battery packs containing several Li-Ion cells joined together. These batteries are to be used in Hilti power tools exclusively. When using Hilti power tools, use Hilti original battery packs!Hilti batteries are state of the art and are equipped with cell management and cell protection systems.
DescriptionThe batteries are composed of cells that contain lithium-ion storage materials that are capable providing high specific energy density. Unlike NiMH and NiCd batteries, Li-ion batteries have a minimal memory effect, but they are extremely susceptible to external impact, deep discharge, and high temperatures. See Safety WARNING
Find our battery-powered products at your Hilti Store or at:
www.hilti.group | USA: www.hilti.com
Safety
- Batteries must not be modified or tampered with!
- Never use recycled or repaired batteries conducted by non-Hilti companies.
- Do not use or charge batteries that have suffered mechanical impact, have been dropped from a height or show signs of damage. Examine your batteries regularly for signs of damage, such as shredding, cuts or punctures.
- Never use the battery or a battery-operated power tool as a hammer.
- Avoid eye or skin contact with leaking liquids!
- See What to do in case of damaged batteries
- Damaged batteries can leak fluid which may moisten adjacent objects. Clean these objects with warm soapy water and replace the damaged batteries.
- See What to do in case of damaged batteries
- Never expose batteries to elevated temperature, sparking, or an open flame because the battery may explode.
- Do not touch the battery poles with your fingers, tools, jewelry, or other metallic objects because this may cause a short circuit, electrical shock, burns or explosions.
- Keep batteries away from rain or moisture. Penetrating moisture can cause short circuits, electrical shock, burns or explosions.
- Only use chargers and power tools approved for the specific battery type. Read and follow the instructions in the respective user manuals.
- Do not store or use the battery in explosion-prone environments containing combustible liquids or gases. An unexpected battery malfunction can cause an explosion under those conditions.
- If a Hilti battery is found to be damaged, contact your Hilti service partner.
- If a battery is leaking, use safety goggles and gloves to avoid direct eye or skin contact.
- To store a damaged battery, place the battery in a non-flammable container and cover the battery with dry sand, chalk powder (CaCO3) or silicate (Vermiculite). Then, close the lid air-tight and store the container away from flammable gases, liquids, or objects.
- Dispose of the container at your Hilti Store , or consult your local governmental garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
- Use a chemical spill cleanup kit to remove leaked battery fluid.
- Watch for abnormal battery behavior, such as faulty charging or unusually long charging times, noticeable power loss, unusual charger LED activity, or leaking fluids. These are signs of an internal problem.
- If you suspect an internal battery problem, contact your Hilti service partner.
- Should the battery be in operational or no longer chargeable or leaking fluid, dispose of it as described above.
- See What to do in case of damaged batteries .
- Provide sufficient venting to permit hazardous and potentially explosive fumes to escape.
- Leave the room immediately in case of intense smoke emission.
- Consult a doctor in case of any skin or respiratory irritation.
- Battery fires should be extinguished with water. Powder fire extinguishers and fire blankets are ineffective with Li-Ion batteries. Fires started by a lithium-ion battery in nearby materials can be extinguished with any appropriate extinguishing agent.
- Do not try to move large quantities of damaged, burning, or leaking batteries. Instead, remove surrounding materials and isolate the batteries. If the scale of the fire is larger than can be extinguished with available methods, contact the nearest firefighting authority.
- Scoop the battery up with a shovel and drop it into a bucket of water, which will reduce the risk of igniting adjacent cells that have not yet reached run-away temperature.
- Wait for the battery to cool down completely.
- See What to do in case of damaged batteries .
- Ambient operating temperature to be kept between -17°C and +60°C / 1°F and 140°F.
- Storage temperature to be kept between -20°C and +40°C / -4°F and 104°F.
- Do not store batteries on the charger. Separate battery from charger after use.
- Store batteries in a cool and dry place. Cool storage will increase battery life. Never store batteries where they are exposed to direct sunlight, on sources of heat or behind glass.
- Batteries should not be sent through the mail. Consult your shipper for instructions on how to ship undamaged batteries.
- Do not transport batteries in bulk, loosely packaged. During transport, batteries should be protected from excessive shock and vibration and isolated from any conductive materials or other batteries that may come in contact with the terminals and cause a short circuit.
- Keep the battery free of oil and grease. If the battery is exposed to oil or grease, remove the contamination with a clean dry rag.
- Never use a battery with clogged venting slots. Clean the venting slots carefully with a soft brush to prevent debris from entering the battery.
- Prevent unnecessary exposure of the battery to dust or debris and never subject the battery to soaking moisture (e.g., submerged in water or left out in the rain).
- If the battery becomes dirty, clean it with a soft brush or clean, dry rag.
- If a battery is exposed to soaking moisture, treat it as a damaged battery and isolate it in a non-flammable container.
- See What to do in case of damaged batteries
- Improper disposal may cause health hazards from leaking gases or fluids. Dispose of the battery at your Hilti Store , or consult your local garbage disposal or public health and safety resources for disposal instructions. Do not ship or mail damaged batteries!
- Do not dispose of batteries as household waste.
- Dispose of your battery out of the reach of children. Cover the terminals with a non-conductive material (such as electrical tape) to prevent short circuiting.